Part Number: TLV320AIC3101
Other Parts Discussed in Thread: TLV320AIC31
最近在海思SS528平台上调试TLV320AIC3101的驱动,硬件做了一路MIC输入、一路LINE IN 输入和一路LINE OUT,原理图如下:

调试了好久,一直没有声音输出,我的寄存器配置:
void soft_reset(unsigned int chip_num)
{
// soft reset
tlv320aic31_write(IIC_device_addr[chip_num], 1,0x80);
msleep(10);
/*CLKDIV_IN uses MCLK*/
tlv320aic31_write(IIC_device_addr[chip_num], 102, 0x32);
#if 1
/*PLL disable and select Q value*/
tlv320aic31_write(IIC_device_addr[chip_num], 3, 0x10);
#else
// PLL enable
tlv320aic31_write(IIC_device_addr[chip_num], 3, 0x81);/* P=1 Q=16*/
tlv320aic31_write(IIC_device_addr[chip_num], 4, 0x20);/* J=8 */
tlv320aic31_write(IIC_device_addr[chip_num], 5, 0x00);
tlv320aic31_write(IIC_device_addr[chip_num], 6, 0x00);
#endif
// left and right DAC open
tlv320aic31_write(IIC_device_addr[chip_num], 7, 0x0a);/* 48 kHz */
// sample
tlv320aic31_write(IIC_device_addr[chip_num], 2, 0xaa);/* FS = FSref/6 */
// ctrl mode
tlv320aic31_write(IIC_device_addr[chip_num], 8, 0x00);/* slave mode */
// Audio Serial Data Interface Control
tlv320aic31_write(IIC_device_addr[chip_num], 9, 0x07);/* I2S mode,16bit */
// Data offset = 0 bit clocks
tlv320aic31_write(IIC_device_addr[chip_num], 10, 0x00);
// Audio Codec Digital Filter Control Register
tlv320aic31_write(IIC_device_addr[chip_num], 12, 0x50);
tlv320aic31_write(IIC_device_addr[chip_num], 14, 0x00);
// The ADC PGA is not muted.
tlv320aic31_write(IIC_device_addr[chip_num], 15, 0x00);
tlv320aic31_write(IIC_device_addr[chip_num], 16, 0x00);
// LINE2L connected to the left ADC PGA
tlv320aic31_write(IIC_device_addr[chip_num], 17, 0x0f);
// LINE2R connected to the right ADC PGA
tlv320aic31_write(IIC_device_addr[chip_num], 18, 0xf0);
// LINE1LP is configured in single-ended mode
// LINE1L connected to the left-ADC PGA
// Left-ADC channel is powered up
tlv320aic31_write(IIC_device_addr[chip_num], 19, 0x04);
// LINE1RP is configured in single-ended mode
tlv320aic31_write(IIC_device_addr[chip_num], 21, 0xC0);
// LINE1RP is configured in single-ended mode
// LINE1R connected to the right-ADC PGA
// Right-ADC channel is powered up
tlv320aic31_write(IIC_device_addr[chip_num], 22, 0x04);
// LINE1LP is configured in single-ended mode
tlv320aic31_write(IIC_device_addr[chip_num], 24, 0xC0);
// Left DAC is powered up
// Right DAC is powered up
// HPLCOM is configured as independent single-ended output
tlv320aic31_write(IIC_device_addr[chip_num], 37, 0xe0);
// HPRCOM is configured as independent single-ended output
tlv320aic31_write(IIC_device_addr[chip_num], 38, 0x10);
// Left-DAC output selects DAC_L1 path,
// Right-DAC output selects DAC_R1 path
tlv320aic31_write(IIC_device_addr[chip_num], 41, 0x00);
// PGA_L is routed to HPLOUT
tlv320aic31_write(IIC_device_addr[chip_num], 46, 0x80);
// DAC_L1 is routed to HPLOUT
tlv320aic31_write(IIC_device_addr[chip_num], 47, 0x80);
// PGA_R is routed to HPLOUT
tlv320aic31_write(IIC_device_addr[chip_num], 49, 0x00);
// DAC_R1 is routed to HPLOUT
tlv320aic31_write(IIC_device_addr[chip_num], 50, 0x00);
// HPLOUT is not muted, HPLOUT is fully powered up
tlv320aic31_write(IIC_device_addr[chip_num], 51, 0x0f);
// PGA_L is routed to HPLCOM.
tlv320aic31_write(IIC_device_addr[chip_num], 53, 0x00);
// DAC_L1 is routed to HPLCOM
tlv320aic31_write(IIC_device_addr[chip_num], 54, 0x80);
// PGA_R is routed to HPLCOM
tlv320aic31_write(IIC_device_addr[chip_num], 56, 0x00);
// DAC_R1 is routed to HPLCOM
tlv320aic31_write(IIC_device_addr[chip_num], 57, 0x00);
// HPLCOM is not muted, HPLCOM is fully powered up
tlv320aic31_write(IIC_device_addr[chip_num], 58, 0x0f);
// PGA_L is routed to HPROUT
tlv320aic31_write(IIC_device_addr[chip_num], 60, 0x80);
// DAC_L1 is routed to HPROUT
tlv320aic31_write(IIC_device_addr[chip_num], 61, 0x80);
// PGA_R is routed to HPROUT
tlv320aic31_write(IIC_device_addr[chip_num], 63, 0x00);
// DAC_R1 is routed to HPROUT
tlv320aic31_write(IIC_device_addr[chip_num], 64, 0x00);
// HPROUT is not muted, HPROUT is fully powered up
tlv320aic31_write(IIC_device_addr[chip_num], 65, 0x0f);
// PGA_L is routed to HPRCOM
tlv320aic31_write(IIC_device_addr[chip_num], 67, 0x00);
// DAC_L1 is routed to HPRCOM
tlv320aic31_write(IIC_device_addr[chip_num], 68, 0x80);
// PGA_R is routed to HPRCOM
tlv320aic31_write(IIC_device_addr[chip_num], 70, 0x00);
// DAC_R1 is routed to HPRCOM
tlv320aic31_write(IIC_device_addr[chip_num], 71, 0x00);
// HPRCOM is not muted, HPRCOM is fully powered up
tlv320aic31_write(IIC_device_addr[chip_num], 72, 0x0f);
// The left-DAC channel is not muted.
tlv320aic31_write(IIC_device_addr[chip_num], 43, 0x80);
// The right-DAC channel is not muted
tlv320aic31_write(IIC_device_addr[chip_num], 44, 0x80);
}
不知道我的这个寄存器配置与我的硬件原理图是否匹配吗?