Part Number: TPA3255
目前在使用TPA3255这颗IC时,IC输出端未接负载给IC供电,IC发热厉害,温度最高能到80摄氏度左右,把后面的LC电路去掉也是一样。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
去掉LC之后,发热没有降低是吗?
是否有触发FAULT和CLIP_OTW拉低?
TPA3255顶部有散热焊盘,是否有使用散热器?
抱歉回复晚了,我们可以通过热阻计算下芯片的结温(测量下supply current,以及output current计算下总功率)和测量的是否相符:
Tj=TA + thetaJA*Pout
TPA3255的热阻挺高的,每输出1W功率温度上升50.7度

在热阻下面有这样的备注:
散热器温度为85°C 时、使用热导率为0.7W/mK 和和2mil 厚度热化合物, 在该模型中,散热器温度被视为环境温度,且散热的唯一路径是
散热器