This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3204: 我配置了ADC的寄存器,只有BLCLK,WCLK的频率是对的,在示波器上看到的DOUT波形是96hz的波形,不知道是哪里配置错了

Part Number: TLV320AIC3204


这是我的寄存器配置

MCLK=24.576MHZ,WCLK=3.072MHZ,BCLK=48KHZ,AIC3204处于主模式,给FPGA提供WCLK和BCLK

# 寄存器 写入数据

0x00,0x00   // Initialize to Page 0

0x01,0x01   // S/W Reset to initialize all registers

 

0x0b,0x81   // Power up NDAC divider with value 1

0x0c,0x84   // Power up MDAC divider with value 4

0x0d,0X00  // Program OSR for DAC to 128(MSB)

0x0e,0X80  // Program OSR for DAC to 128(LSB)

0x12,0x81   // Power up NADC divider with value 1

0x13,0x84   // Power up MADC divider with value 4

0x14,0x80   // Program OSR for ADC to 128

0x19,0x00   //Select CODEC_CLKIN = MCLK      

0x1b,0x3c   // Set the word length of Audio Interface to 32bits,BCLK,WCLK is output from the device

0x1c, 0x00  // Data Offset = 0 BCLKs

0x1d, 0x06  // BDIV_CLKIN = ADC_CLK

0x1e, 0x88  // Power up BCLK divider with value 8

0x3c,0x04   // Select DAC PRB_P4

0x3d,0x01   // Select ADC PRB_R1

 

 

0x00,0x01   // Select Page 1

0x01,0x08   // Disable Internal Crude AVdd in presence of external AVdd supply or before powering up internal AVdd LDO

0x02,0x00   // Enable Master Analog Power Control

0x14,0x25    //HP soft stepping settings for optimal pop performance at power up

                    //Rpop used is 6k with N = 6 and soft step = 20usec. This should work with 47uF coupling

                   //capacitor. Can try N=5,6 or 7 time constants as well. Trade-off delay vs “pop sound.

0x0a,0x00   // Set the input common mode to 0.9V

                  

/*---Analog Routing---*/

0x0c,0x08   //Route Left DAC to HPL

0x0d,0x08   //Route Right DAC to HPR

0x0e,0x08   //Route Left DAC to LOL

0x0f,0x08    //Route Right DAC to LOR

0x03,0x00   //Set the DAC PTM mode to PTM_P3/4

0x04,0x00   //Set the DAC PTM mode to PTM_P3/4

0x3d,0x00   // Select ADC PTM_R4

0x10,0x00   //Set the HPL gain to 0dB

0x11,0x00   //Set the HPR gain to 0dB

0x12,0x00   //Set the LOL gain to 0dB

0x13,0x00   //Set the LOR gain to 00dB

0x09,0x3c   //Power up HPL and HPR, LOL and LOR drivers

//Wait for 2.5 sec for soft stepping to take effect

                //Else read Page 1, Register 63d, D(7:6). When = “11” soft-stepping is complete

0x47,0x31   // Set MicPGA startup delay to 3.1ms

0x7b,0x01   // Set the REF charging time to 40ms

0x34,0x80   // Route IN1L to LEFT_P with 20K input impedance

0x36,0x80   // Route Common Mode to LEFT_M with impedance of 20K

0x37,0x80   // Route IN1R to RIGHT_P with input impedance of 20K

0x39,0x80   // Route Common Mode to RIGHT_M with impedance of 20K

0x3b,0x0c   // Unmute Left MICPGA, Gain selection of 6dB to make channel gain 0dB

// Register of 6dB with input impedance of 20K => Channel Gain of 0dB

0x3c,0x0c   // Unmute Right MICPGA, Gain selection of 6dB to make channel gain 0dB

// Register of 6dB with input impedance of 20K => Channel Gain of 0dB

 

0x00,0x00   // Select Page 0

0x3f,0xd6    //Power up the Left and Right DAC Channels with route the Left Audio digital data to

                //Left Channel DAC and Right Audio digital data to Right Channel DAC

0x40,0x00   //Unmute the DAC digital volume control and enable syncronized control (use L-ch)

0x51,0xc0   // Power up Left and Right ADC Channels

0x52,0x00   // Unmute Left and Right ADC Digital Volume Control.