This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我升级到linux5.15.71配置声卡的时候,选配了snd-soc-tlv320aic3x.ko 和 snd-soc-tlv320aic3x-i2c.ko 模块,安装完成后
ls /dev/snd/ by-path controlC0 pcmC0D0c pcmC0D0p timer
但是安装完模块后 i2c命令无法使用,不安装模块时都是可以使用的
# i2cdump -y -f 0 0x18
No size specified (using byte-data access)
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXX
无论是播放还是录制音频都是显示这种信息
c# aplay sine.wav
Playing WAVE 'sine.wav' : Signed 32 bit Little Endian, Ra[ 1101.900499] fsl-sai 2028000.sai: failed to derive required Tx rate: 2822400
te 44100 Hz, Stereo
[ 1101.909754] fsl-sai 2028000.sai: ASoC: error at snd_soc_dai_hw_params on 2028000.sai: -22
[ 1101.923524] 2028000.sai-tlv320aic3x-hifi: ASoC: soc_pcm_hw_params() failed (-22)
aplay: set_params:1297: Unable to install hw params:
ACCESS: RW_INTERLEAVED
FORMAT: S32_LE
SUBFORMAT: STD
SAMPLE_BITS: 32
FRAME_BITS: 64
CHANNELS: 2
RATE: 44100
PERIOD_TIME: (125011 125012)
PERIOD_SIZE: 5513
PERIOD_BYTES: 44104
PERIODS: 4
BUFFER_TIME: (500045 500046)
BUFFER_SIZE: 22052
BUFFER_BYTES: 176416
TICK_TIME: 0
在我安装模块时,有这样一个错误
# insmod snd-soc-tlv320aic3x-i2c.ko
[ 327.413410] tlv320aic3x 0-0018: Unsuitable MicBias voltage found in DT
下面是我的相关设备树配置
sound { compatible = "simple-audio-card"; simple-audio-card,name = "tlv320aic3104"; simple-audio-card,format = "i2s"; simple-audio-card,mclk-fs = <256>; simple-audio-card,bitclock-master = <&dailink0_master>; simple-audio-card,frame-master = <&dailink0_master>; simple-audio-card,widgets = "Microphone", "Microphone Jack", "Headphone", "Headphone Jack", "Speaker", "External Speaker", "Line", "Line Out", "Line", "Line In"; ,routing = "MIC_IN", "Microphone Jack", "Headphone Jack", "HP_OUT", "LINE1L", "Line In", "LINE1R", "Line In", "Headphone Jack", "RLOUT", "Headphone Jack", "LLOUT"; dailink0_master:simple-audio-card,cpu { sound-dai = <&sai1 0>; }; simple-audio-card,codec { sound-dai = <&codec 0>; // clocks = <&clks IMX6UL_CLK_SAI1>; }; }; &sai1 { #sound-dai-cells = <0>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_sai1>; assigned-clocks = <&clks IMX6UL_CLK_SAI1_SEL>, <&clks IMX6UL_CLK_SAI1>; assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>; assigned-clock-rates = <2>, <24576000>; status = "okay"; }; &i2c1 { clock-frequency = <100000>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_i2c1>; status = "okay"; codec: tlv320aic3104@18 { #sound-dai-cells = <0>; compatible = "ti,tlv320aic3104"; reg = <0x18>; gpio-reset = <&gpio1 26 GPIO_ACTIVE_LOW>; ai3x-micbias-vg = <0>; /* Regulators */ DRVDD-supply = <®_3p3v>; AVDD-supply = <®_3p3v>; IOVDD-supply = <®_3p3v>; DVDD-supply = <®_1p8v>; status = "okay"; };
请问我是哪里没配置,还有有什么配置错误呢?menuconfig里面选配那些
您好,
您在哪里找的的snd-soc-tlv320aic3x.ko 和 snd-soc-tlv320aic3x-i2c.ko?
看下面FAQ有提到TLV320AIC3104 驱动,看下是否有帮助:
[FAQ] Linux Drivers: Device drivers for AIC31xx/DAC31xx/AIC325x/AIC320x/AIC326x/AIC321x
这个链接的驱动文件安装后,显示找不到声卡。我编译我自己的内核,如果能找到声卡就无法使用i2ctool工具,也无法播放和录制。和声卡是冲突的,是不是我的设备树那里配置有问题呢,但是我没有查看到错误
root@:/music# i2cdump -y -f 0 0x18
No size specified (using byte-data access)
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXX
10: XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XXXXXXXXXXXXXXXX
很抱歉现在才回复您的问题,我不懂linux,为更好解决您的问题,建议您将问题发布在E2E英文技术论坛上,请资深的英文论坛工程师为您提供帮助,英文论坛对应子论坛链接:https://e2e.ti.com/support/audio-group/audio/f/audio-forum