Other Parts Discussed in Thread: TLV320AIC3101, TLV320AIC3104
大家好!小弟最近在用TLV320AIC3101这款芯片。目前通过LINE2 输入 PGA+ADC (关掉了AGC)+DOUT,然后DOUT直接送给DIN+DAC+HPLOUT的方式。目前PGA的增益设置为0dB。输入为一200mV的1khz的单频正弦波。输出时候发现正弦波上面叠加了许多高频分量。导致失真度很大。必须通过仪器自带的低通滤波器后方能得到较好的单频正弦波。测试仪器的低通滤波器为80KHZ截止频率。我手上现在没有TLV320AIC3101的开发板。我想问一下DAC通道的声效滤波器能否进行低通滤波处理。我的采样率为44100Hz。如果能够进行低通滤波处理,那么滤波器参数怎么进行设置。希望大侠手上有开发板以及软件计算工具的提供一下给我谢谢
!能够带上寄存器设置更好。稍后我会把我的寄存器设置值附上。希望TI的工程师能够回答一下我的问题,谢谢。不甚感激1