This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3123D2: 刚上电时,正常。播放过一次语音后,静态电流增大,芯片会发烫。大概有近1W功耗在发热。

Part Number: TPA3123D2


原理图见上图。5,6脚输入,由语音合成芯片产生。电源是DC12V。右侧输出接8Ω/12W喇叭。

当刚上电时,电流一切正常,TPA3123芯片不发热。当播放过一次语音后,静态电流增大,功耗比刚上电时大了近1W左右。尝试过去掉输入,尝试过去掉输出端的E11和E12电容,尝试过改变C20/C25,C17/C22电容大小,都没有改变。用示波器测试21和22脚的输出,发现有差不多200KHz的左右的波形输出,幅值略小于12V(刚上电时,没有输出)。打样了一批板子,出现的概率在80%左右。研究了很久的芯片资料以及参考电路,都没有找到思路。求助!!急!

  • 您好,

    明天或后天我会具体看下你的问题,若给你带来不便很抱歉。

  • 首先很抱歉现在才回复你的问题。看下是不是输出功率太大把喇叭烧坏了?建议降低输出功率,且换个新的喇叭再做测试看现象怎样?

  • 刚才回复了,可能网络不好,没成功。重新发一次。。。喇叭没有烧坏,是正常的。测试了好多台机器,都有这个问题。刚上电时,输出15、22脚没有波形;当放过一次声音后,15、22脚就有波形输出。即使断开输入端,断开喇叭,15、22脚都有输出,导致功耗增大。正常播放声音时,芯片反而不热;停止播放声音后,芯片发烫,甚至出现过热断音现象。

  • 急等解决问题。好多天了,也没消息。有没有电话可以实时联系啊,急等解决问题!