This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助!!TP3067!!

最近在做课程设计,做一个和之前通信实验用的芯片一样的PCM模块。用的是TP3067,原理图如下:

时钟信号产生电路:

主时钟:2.048MHz

位时钟:2.048MHz

帧同步信号:8KHz

以下是8K时钟和2048K时钟,不过振铃有点厉害不知道有没有影响。而且接上电路之后,变得更加糟糕。

PCM编码输出:

当信号是2K的时候,输出波形是可以接受的。

在实验室做的时候,下限可以到300Hz左右,不过我做出来到1.3K左右就开始变形了。