This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在使用TPA3110做一款产品,只需要输入固定频率不同幅度的信号,信号范围在28KHz左右。
但是现在出现一个问题就是,在/SD 使能前,如果RINP已经有一个幅度稍微大点的信号,功放使能时就会自动保护,然后400mS后又使能,然后又保护。如此反复。
目前处理是,/SD使能后,延时25mS,然后输入信号,且信号幅度按一定步进缓慢增加。此点导致要到达需要的初始输入,需要120多mS。反应太慢。
在使能后的使用过程,需要改变幅度时,也只能采用幅度缓慢变化的方式,否则功放又会自动保护掉。从最小一档到最大一档,这种方式需要500mS左右,影响使用感觉。
谢谢XP,我昨天按你说的,用5欧姆和2.5欧姆的功率电阻分别串如回路试了一下,幅度变化较大时,的确没有保护。不过我的功率受了点影响。XP 说:亲;你的变压器负载太小。如果不增加损耗解决问题,建议前级加低通;滤除18kHz以上信号。
另外,这个方案板上还要留出大功率电阻的位置,就我目前设计有点困难。
引起这个现象的,难道是瞬间变化较大时,我的滤波器,变压器电感出现饱和,变导线了吗?不是很理解,我滤波器电感是10A的。
另外,我的应用频率是28KHz,滤波器是滤除32KHz以上的频率。
我今天再试试电阻减小到多少还可以。