Part Number: TLV320AIC3104
TLV320AIC3104IRHBR现在遇到了这种情况,我的LINE_IN输入20hz频率的音频数据经过3104之后声音的DB变减少了很多,但是我输入1000hz的频率的音频就没有消减多少。请问是什么导致的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV320AIC3104
TLV320AIC3104IRHBR现在遇到了这种情况,我的LINE_IN输入20hz频率的音频数据经过3104之后声音的DB变减少了很多,但是我输入1000hz的频率的音频就没有消减多少。请问是什么导致的?
您好
频率响应是音频编解码器的一个重要性能指标,它决定了不同频率信号在经过编解码器处理后的衰减情况。TLV320AIC3104作为一款低功耗立体声音频编解码器,其设计初衷是覆盖较宽的音频频率范围,但具体的频率响应特性可能会受到多种因素的影响,包括电路设计、元件选择以及软件配置等。
对于20Hz这样的低频信号,出现较大衰减的可能原因包括:
相比之下,1000Hz这样的高频信号在传输和处理过程中可能受到的影响较小,因为高频信号通常对电路中的非理想因素(如电容、电感等)的敏感度较低。此外,高频信号也可能更容易通过滤波器而不被显著衰减。