This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在使用TAS2781 EVM评估板测试,发现没有达到规格书中说的25 W, 1% THD+N (4 Ω, 18 V),目前测试到时最大2W左右,供电是直流电源18V,使用的喇叭是4欧姆40W的,音源使用的是1KHz 0dB,音量条设置到最大,但是不知道是什么原因还是达不最大功率的理论值,甚至相差很远!