This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6133A2: TPA6133A2总功耗如何计算

Part Number: TPA6133A2


TPA6133A2总功耗如何计算?

规格书中有IQ=4.2mA, 假设3.6V供电,左右声道各有一个32ohm的喇叭,每个喇叭5mW的输出,芯片供功耗是多少?

计算过程:

1.芯片自身消耗IQ=3.6V;

2.每个喇叭的消耗:Ispk=√(5mW/32ohm)=12.5mA

3.两个喇叭的消耗:Ispk(2)=Ispk*2=25mA;

4.总功耗=IQ+Ispk(2)=29.2mA.

问题:

1.以上计算芯片消耗是否正确?

2.IQ=4.2mA 是不是意味着,芯片只要一上电,使能,不管没有输出,都会消耗4.2mA的电流?