register config in next picture.

and i read from state register.

i config I2S bclk is 48000hz and bclk/FSYNC is 64,reg 0x15 = 0x44 is correct.
is there something wrang in reg config?
please give me some advise.
linyong0321@gmail.com

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
register config in next picture.

and i read from state register.

i config I2S bclk is 48000hz and bclk/FSYNC is 64,reg 0x15 = 0x44 is correct.
is there something wrang in reg config?
please give me some advise.
linyong0321@gmail.com

The device configuration script seems to be correct.
1) Can you also check the status of the two interrupts in the INT_LTCH0 register?
2) Is there no PDMCLK seen when probing the PDMCLK pins of the PCMD3180 on a scope?
3) Is this systematically seen on multiple PCBs?
Long time no reply received, this post is closed