I configured the LMK04208EVM evaluation board with the following settings, but found that there is a deviation between the actually measured clock and the clock displayed in the TICS Pro software.
R0 (INIT) 0x00160040
R0 0x001400A0
R1 0x00140281
R2 0x001400A2
R3 0x001400A3
R4 0x40140084
R5 0x001400A5
R6 0x0C600006
R7 0x01100007
R8 0x01060008
R9 0x55555549
R10 0x9642560A
R11 0x0001100B
R12 0x1B0C006C
R13 0x3B13924D
R14 0x1300000E
R15 0x8000800F
R16 0xC1550410
R24 0x00000058
R25 0x02C9C419
R26 0xAFA8001A
R27 0x1000065B
R28 0x0020191C
R29 0x0180003D
R30 0x0500003E
R31 0x003F001F
test result
oscout=122.85MHz
clkout0=107.29MHz
clkout1=26.8MHz
clkout2=107.29MHz
clkout3=107.29MHz
clkout4=30.721MHz
clkout5=107.29MHz
All measured values show deviations from the theoretical values except for CLKOUT4.
When configured on our own development board, there is no clock output from CLKOUT0 to CLKOUT5.
I feel very strange, hope your response as soon as possible. Thanks!