This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2491: lmx2491寄存器配置与相关细节问题,我的目的是在外部vco的输出端接收到5.5~6.1GHz的线性调频信号

Part Number: LMX2491

你好,对于这个问题我有新的疑问,你能帮我看看吗,谢谢

1、首先是对整个流程的解读,是不是反馈的信号经过N分频器后和经过R分频器的信号不断地进行相位比较,在cpout口输出一个电流信号,电流信号经过外部的环路滤波就是变成电压信号,相应的电压斜坡信号再经过外部的vco得到对应的频率斜坡信号(我这个例子中是5.5~6.1GHz的线性调频信号)

2、对于寄存器信息配置部分,下面的图1会对我的斜坡波形(图2)有所影响吗,因为我的目的是在vco的输出部分得到一个5.5~6.1GHz的信号,而不是单频信号。然后图1环路滤波器的末端应该是得到一个通过200微秒计算得到的5kHz的电压斜坡波形是吗,还是说是一个65MHz相关的信号

3、我像图2那样配置是在cpout就输出一个线性调频波还是在外部vco后面才输出线性调频波

image.png

4、我是通过spi来通信的,vivado仿真的波形如图,写24个数据后就缓冲,再写24个数据,这有什么错误吗

5、如果我想要验证,有什么方法吗,因为我现在示波器测出来的有点怪