Part Number: LMK04828
Hello,
I have a question about the recommended AC-coupled LVDS input connection for LMK04828.
In the datasheet, the 100 Ω differential resistor is placed before the AC coupling capacitors. But in many other LVDS application notes and reference designs, the 100 Ω termination is usually placed after the capacitors, near the receiver.
Could you please help explain why LMK04828 uses this different connection method?
Is it because the LMK04828 input has internal biasing, so the resistor is mainly used to provide the proper load for the LVDS driver rather than acting as a conventional receiver-side termination?
Also, what would happen if the 100 Ω resistor were placed after the AC coupling capacitors near the LMK04828 input instead?
Thank you.