Other Parts Discussed in Thread: LMX2595, LMX2572
您好!
我在LMX2595的使用过程中,参考频率100MHz,鉴相频率100MHz,三阶小数模式,输出13~19GHz,25MHz步进。当VCO设置成Full assist下,切换频点时发现,部分频点偶尔有杂散偶尔没有。杂散见附图1/2,寄存器值设置见附图3。而当VCO设置成Partial assist或No assist 模式时不会出现杂散。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
好的,麻烦您了!
我之前在使用LMX2572的时候也有同样的问题,只是杂散幅度有65dBc左右,我就没管了。所以现在还是特别想知道是怎么回事的。而且现在产品货期还是比较急的。
您好,麻烦您把寄存器配置以.txt方式附上。
另外,能举例是在哪些频点出现的杂散吗?
R78 0x4E0003 R77 0x4D0000 R76 0x4C000C R75 0x4B0800 R74 0x4A0000 R73 0x49003F R72 0x480001 R71 0x470081 R70 0x46C350 R69 0x450000 R68 0x4403E8 R67 0x430000 R66 0x4201F4 R65 0x410000 R64 0x401388 R63 0x3F0000 R62 0x3E0322 R61 0x3D00A8 R60 0x3C0000 R59 0x3B0001 R58 0x3A8001 R57 0x390020 R56 0x380000 R55 0x370000 R54 0x360000 R53 0x350000 R52 0x340820 R51 0x330080 R50 0x320000 R49 0x314180 R48 0x300300 R47 0x2F0300 R46 0x2E07FE R45 0x2DD0C0 R44 0x2C0AA3 R43 0x2B0753 R42 0x2A0000 R41 0x290000 R40 0x280000 R39 0x2707D0 R38 0x260000 R37 0x250404 R36 0x240027 R35 0x230004 R34 0x220000 R33 0x211E21 R32 0x200393 R31 0x1F43EC R30 0x1E318C R29 0x1D318C R28 0x1C0488 R27 0x1B0003 R26 0x1A0DB0 R25 0x190C2B R24 0x18071A R23 0x17007C R22 0x160001 R21 0x150401 R20 0x14CC48 R19 0x13275B R18 0x120064 R17 0x11012C R16 0x1000DE R15 0x0F064F R14 0x0E1E70 R13 0x0D4000 R12 0x0C5001 R11 0x0B0018 R10 0x0A10D8 R9 0x091604 R8 0x086800 R7 0x0740B2 R6 0x06C802 R5 0x0500C8 R4 0x040A43 R3 0x030642 R2 0x020500 R1 0x010808 R0 0x002514
这是100MHz参考,200MHz鉴相,输出15.975GHz时的寄存器表!这个频点出现杂散概率较大。而且一旦有频点出现杂散,切换到其他本来没有杂散的频点,也会变的有杂散。
为什么LMX2595/LMX2572寄存器中没有MASH_DITHER/Dithering功能?那在Full assist模式下遇到小数杂散该怎么办?