This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 请问用5V给NE555供电, 做一个PWM信号发生器,NE555输出信号的高电平是5V吗,还是3.3V.
2. 第5脚可以悬空吗。
您好,
看数据手册7.4Electrical Characteristics 表格,在5V供电时High-level output voltage典型值是3.3V。
抱歉,第二问忘记回复了
看datasheet如下截图,CONT对地接电容可以提高性能,悬空的话应该也可以
我用Proteus 仿真结果输出是5V。不知道是不是模型不一样。
555是推挽输出,上管是达林顿双管,输出高电平时需要减去2个管子(约2*0.7V)的压降;另外模型并不能完全反应器件的实际性能
谢谢回复,先做一个样品实验一下。