This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM7005: PLLVCO状态指示异常

Part Number: CDCM7005

原理图接法:

VCO指标:

输出频率:384MHz

输出功率:1.5~4.5dBm

调谐电压0.5~2.5V

压控灵敏度:3-6MHz/V

PLL设置:

输出时钟:384MHz,96MHz,24MHz

参考时钟:100MHz

问题:六块板卡有两块的板卡的CDCM7005芯片,STATUS_VCO状态指示管脚,在低温-10度时,STATUS_VCO状态指示异常,锁定指示也异常,但测试芯片的输出时钟384MHz,96MHz,24MHz无问题,证明锁相环锁定正常,仅状态指示异常。常温无任何问题。

改环路带宽为100K,问题仍然存在。

手册上查不到,STATUS_VCO状态指示的内部电路,不清楚问题出在哪?

VCO为单端输出,接到锁相环芯片的VCXO_IN+管脚,datasheet中并没有单端输入的接法说明,请问这种接法对么?

  • 您好,

    您使用的是CDCM7005吗?CDCM7005只有48 pin  VQFN封装和64pin BGA封装,我看原理图中是52pin的,管脚名称也对应不上

  • 我用的是cdcm7005-sp V级 陶瓷封装的 你说的那个是塑封的

  • 对于VCXO_IN的单端输入,您是输入的LVCMOS信号吗,如果是LVCMOS信号这样接没问题,如果VCXO是LVPECL输出类型,则可将其直接直流耦合至CDCM7005 VCXO输入;

    关于STATUS_VCO指示状态异常,数据手册P11下方有以下说明 ,即 如果反馈时钟(源自VCXO输入)小于2 MHz,则设备保持在正常工作模式,但频率检测电路将STATUS_VCXO信号和PLL_LOCK信号置低。两个状态信号不再相关。这也会影响HOLD-over功能,因为PLL_LOCK信号不再有效!  因此,在指示状态异常时,您检查下这个反馈时钟Feedback Clock是否有可能小于2 MHz?

  • 我的VCO时钟是单端的384MHz输出,输出阻抗是50欧姆,我测试过VCO输出是384MHz没有问题,在STATUS_VCO异常时,五路锁相环芯片输出时钟频率正确,且频漂在2Hz以内,时钟输出正常,这证明VCO输出频率是没有问题的,仅仅是STAYUS_VCO状态指示异常,锁定指示也异常。

  • feedback clock 如下图所示,您可以确认下这个反馈频率是否大于2MHZ?

    如果是大于2MHZ的,您可以分享出您的配置文件吗?以查看问题