Other Parts Discussed in Thread: LMX2572, ,

如上图,VCC是低噪声LDO稳压得到的3.3V,带电流能力没有问题。 实际测试中,如果开2分频,比如输出4500M,每次加电都有概率出现环宽不同的两种情况。一种是正常环路,和仿真值可以拟合;一种是明显变宽的环路。测试中发现,选用不同的MESH ORDER、选用不同的参考功率、选用不同的PFD_DLY,异常情况的环宽有所不同,能够得到改善(和正常环宽比,变化小一些),但是这种情况却始终存在。 实际使用LMX2572时,同样的电路,却没有类似情况。去掉LDO,直接用线性稳压电源加3.3V,情况依旧。反复修改寄存器参数,情况依旧。使用2594的EVM,这种情况基本没有出现,但始终找不到问题,请问有可能是哪里的问题?和外围电路隔离有关吗?