This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NE555: 555做为RS触发器应用

Part Number: NE555

图中J1是可变电阻,测量箭头指向的1处 的阻值,并是不50K,如果J1的阻值变化,1处的阻值也变化,这是什么原因呢?

  • 您好,

    您是测量的哪里的电阻?是1处对GND的电阻吗?您的可变电阻是怎样接的?1处对GND除了R1、R2还有其他对GND回路吗?

    另外请注意下电阻需断电测量

  • 又看了下,1处D2、R5、R6也是一个对GND回路,这可能是造成1处对GND电阻不是50K的原因;

    如果J1的阻值变化,1处的阻值也变化,那可能J1可变电阻处有对GND回路。

    555的TR引脚是比较器输入管脚,其输入阻抗很大的,应该不会对1处对GND电阻造成影响