This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC555-Q1: TLC555-Q1应用问题

Part Number: TLC555-Q1

TLC555-Q1应用电路原理图如下:

问题1:从规格书看R30, R26和C49 决定了时钟的周期和占空比,根据规格书给出的计算公式,可算得f=357.6kHz,高电平占空比为0.59,但我实测发现f=426kHz, 占空比为0.34,即使考虑器件偏差造成得误差也与理论计算的偏差甚大,是什么原因呢?

问题2:我的A样和B样PCBA,原理图完全一样,PCB layout 唯一的区别在于C57的GND平面铺铜更大,但实测结果显示,A样PCBA的TLC555-Q1电路输出时钟周期为460kHz, 占空比为0.12;而B样电路输出时钟周期为426kHz,占空比为0.34,均于理论计算不符,why?  经查,A样和B样的TLC555-Q1供电VP都为15.7V, 唯一不同的是5脚(cont)电平,A样的实测为4.45V,B样的实测为10.43V,不知什么原因能导致?

以上疑惑,麻烦解答,谢谢!

  • 您好,

    建议在100kHz以下的频率下使用555,如下面Figure 9. Free-Running Frequency所示。超过100kHz的频率更难获得良好的精度,在更高的频率下工作,电路板的寄生电容将起到一定的作用。当电容值很小时,电路板寄生电容可能引起较大的误差。

    对于PCB布局中的寄生电容,有一些通用的实践指南可供遵循:

    1、增加相邻走线之间的间距;

    2、关键走线远离电源和地网络;

    3、尽量减小走线长度,因为走线长度越长,寄生电容越大;

    4、关键走线不使用或尽量减少使用过孔。