看NA555DR芯片的规格书,VCC最低电压需要在5V供电,实际我这边PCB上因为只有3.3V电压,我就用3.3V供电搭了个单稳态触发器,发现使用都正常,波形看也没问题,请问这个供电电压值VCC用3.3V确定也可以吗?
因为后面需要批量使用,担心会有其他隐藏问题会导致异常,麻烦给确认下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,不建议脱离数据手册中的电气特性去使用,NA555的供电电压范围为4.5V~16V,最低4.5V,如果不在这个范围内,不能保证芯片的长期性能。
并且所有的电气参数都是在4.5V~16V范围内测试的结果,即使目前3.3V能使用,但不能保证其能长期工作。

您好,虽然3.3V目前能工作,但我们不能确保电压低于数据手册中指定的值芯片会出现什么影响。
对于 NA555,我们建议的最小电源电压为4.5V。当我们指定最小电源时,我们会考虑工艺和温度过高问题。如果应用需要低于4.5V 的电压,我建议使用 TLC555C。TLC555C 的电压低至2V最高可到15V。
Pin2 TRIG的电压为1/3的VCC电压,可以看到当VCC=5V时,范围为1.1V~2.2V ,典型电压为1.67V。
如果VCC=15V,为4.5V~5.6V范围,典型值为5V。
所以如果TRIG需要和MCU的3.3V连接,那么NA555的供电电压VCC=3.3*3=9.9V左右。

而pin3 OUT的输出引脚,当VCC=5V时,OUT输出为3.3V。

所以综上,如果VCC=5V的话,需要pin2=TRIG=1.67V,此时OUT输出3.3V可以和MCU的3.3V接。
不好意思,我的应用可能我没说清楚,我是做单稳态触发器使用,NA555的2脚我是连接的系统MCU的RESET引脚,上拉10K电阻到3.3V,同时NA555的3脚是直接接到MCU的输入口。
正常时:NA555的2脚是3.3V电压输入,NA555的3脚输出低电平
当MCU的RESET引脚有拉低时:会启动NA555进入暂稳态,NA555的3脚输出高电平,NA555的6脚电压根据RC升高到2/3 5V时暂稳态结束,NA555的3脚会回到低电平
所以我的理解是NA555的2脚只要低于1.67V,这个单稳态触发器就会启动暂稳态延时,所以是不是输入3.3V高电平没什么问题了?

您好,2脚低于1/3=1.67V时,触发器被置位。输出为高电平。
当2脚高于1/3Vcc 并且6脚高于2/3VCC电压时,触发器进行reset。输出为低。
我按照您的电路用TINA仿真了下,2脚我使用的0~3.3V的方波模拟您现在接在MCU的reset引脚上,仿真结果您看下,是正常工作的。