本款芯片给我带来极差的调试体验,体现在4脚和23脚的下拉电阻上,1.每次进行配置时,需要先拆下两个电阻,否则I2C通讯会不正常。2.在正常启动时,又需要焊接上两个电阻,实现输入信号和EEPROM的选择。如果配置不对,则需要反复进行操作一操作二,极为麻烦,建议需要用这款芯片的用户慎用
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本款芯片给我带来极差的调试体验,体现在4脚和23脚的下拉电阻上,1.每次进行配置时,需要先拆下两个电阻,否则I2C通讯会不正常。2.在正常启动时,又需要焊接上两个电阻,实现输入信号和EEPROM的选择。如果配置不对,则需要反复进行操作一操作二,极为麻烦,建议需要用这款芯片的用户慎用
我刚刚还发现一个问题,在TICS Pro在关于Pll_ndiv有如下描述:
Description: Ncount value. The actual value will be 4 less than programmed value. Also - during the calibration - the value will 4 times (minus 4) the programmed value. Refer State Machine Document
RW
是否需要根据实际倍数加4去编程呢?

编程时我认为这里不用去更改寄存器Pll_ndiv的值,TICS Pro生成的值是多少编程时就写入多少,您这里实际操作有什么异常吗?
但是,我发现EEPROMSEL = MID REFSEL= low时,I2C也不可用,回读数据都是0000或者FFFF
这种配置没有对应的工作模式,EEPROMSEL = MID 的话,REFSEL也需要为MID ,这样是工作在Fall-Back Mode下:

可以的,这里应该是只列举了一种情况,即分频的情况,分频的话最低只能是1;
倍频只有一种,即2倍频。
这里需要注意的是PFD 频率范围,即 1 MHz to 100 MHz,满足这个范围就可以。