I am 1st time using LMX2594. Input clock is 100MHz, Output required is 1000MHz, But i do not get.
Help check the following parameters:
Doubler:X2
PreR:1
Multiplier:bypass
R:1
FPD:200MHz
N divide:50
Output MUX:VCO
PFD_DLY_SEL:3
RFoutA:10000MHz
Whether the above settings are correct