This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
请教一个问题,当LMK00725的输入为LVPECL电平时,由于芯片输入管脚内部存在51KOhm上下拉,那在芯片外部是否还需要增加上下拉偏置电阻呢?
我目前参考的是手册中的典型应用电路(Datasheet Figure19)进行设计的,100R端接,前端LVPECL输出180R下拉,如下图1,没有预留上下拉偏置电阻。
但检查手册中的Figure11与Figure12,如下图,输入的接法和上图Figure19是不一致的,搞得我有点混乱。。。
确认下手册中这三张图对应的三种接法模式是否都可以工作呢?
请帮忙解答下,感谢!
您好,首先FIGURE19中红色您圈出来的部分,180ohm下拉是为了给直流提供一个回流路径,通常AC耦合的话,需要在driver的输出端下拉电阻到地,也就是像右边Q输出端和10GE PHY的连接方法。
FIGURE11中在接收端加上下拉电阻提供偏置是常用的建立偏置电压的方法,通常也是用于AC耦合,driver和receiver端共模电压不一致,需要在靠近接收端重新建立。但是这里上下拉阻值好像写反了,LVPECL的共模电压是2V,因此84ohm和125ohm电子需要换一下,V={84/(84+125)}*3.3=2V。
下面FIGURE12的图在接收端下拉50ohm相当于给定一定的负载,由于driver和receiver都是LVPECL电平,所以可以直接DC耦合。
这三种应该都是可行的,您在电路设计时可以参考FIGURE19的电路,它给出了具体和clock gen还是输出端和PHY接的方法。