This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCI6214: 采用FPGA配置后,没有时钟输出

Part Number: CDCI6214


您好,我在调试CDCI6214的过程中遇到了一个问题想请教一下。

我想要在4通道输出100MHz的AC-LVPECL的时钟,在1通道输出10MHz的LVDS时钟。在Fallback模式下(EEPROMSEL和REFSEL都去掉电阻悬空)我采用FPGA对CDCI6214进行了寄存器配置,配置数据采用的是TICS PRO中的寄存器配置数据,并且读数据的时候发现数据写入正确,但是测量时钟输出时发现没信号。这种情况应该怎么解决?