This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: LMX2594

Part Number: LMX2594

你好,我现在用的LMX2594做clk输出时发现上位机上设置的clk是10GHz,但是实际测试出来是10.5GHz左右,我测试VBIASVCO电压只有0.3V,在datasheet里描述说是1.3V,请问大约是哪里的原因?做过如下排查:10

0MHz  晶振输入正常,芯片供电电压正常(万用表测试输入VCCBUFFER、VCCVCO、VCCVCO2、VCCMASH、VCCCP、VCCDIG为3.285V);

测试VBIASVCO=0.263V,spec理论值:1.3V,测试购买的DEMO板上也是0.266V

VBIASVCO2=0.634V,spec理论值:0.7V

VREFVCO2=2.814V,spec理论值:2.9V

VBIASVARAC=1.472V,spec理论值:1.7V

VREFVCO=2.813V,spec理论值:2.9V

VREGVCO=1.985V,spec理论值:2.1V

理论值是通过datasheet 64页描述中得到的