This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572: selecting the VCO output,the channel divider couldn't power down

Part Number: LMX2572

When I was using CPLD to configure LMX2572, I encountered the following problem: I was able to switch frequencies below 3.2GHz, but when I tried to switch frequencies above 3.2GHz, I got a Divider output of the frequency I wanted. I configured OUTA_MUX and OUTB_MUX according to the manual, trying to close the Channel Divider, but it didn't seem to work. So I would like to ask you if there is a good solution? (I have seen similar problems on the forums, but it doesn't seem to be solved perfectly)