This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL5010: tpl5010复位问题

Part Number: TPL5010


板卡上DC-DC出来的3V3分别给三个地方供电:

1、单片机;

2、tpl5010;

3、温湿度传感器(电源开启受单片机IO控制);

测试中发现:

     单片机控制温湿度传感器供电开启的瞬间,3V3波形有抖动,Vmax=4.2V(tpl5010 pin1测得),导致tpl5010 RSTn拉低,单片机复位重启;

     其他没有此复位现象的板卡在温湿度传感器供电开启瞬间,3V3也有波动,但幅度较低,Vmax=3.91V;

tpl5010输入电源1.8-5.5V;

前级选取的DC-DC输出3V3、3A,带载能力足够;

请帮忙分析一下这个是什么原因导致的复位?

  • 您好,

    我怀疑是单片机控制温湿度传感器供电开启的瞬间,3.3V供电的抖动耦合到了RSTn pin,造成RSTn 误触发单片机复位。你可以用示波器同时测量3V3供电电压和RSTn pin来验证这一点,看下RSTn pin的信号变动是否与供电3V3同时发生的?