Other Parts Discussed in Thread: LMX2571
您好,我今天尝试了您所说的这些方法,内部VCO已经成功振荡并在频谱仪上有了波形,但是目前的问题是无法锁定,我更改了R4寄存器的N值,但是频率一直没有变化,甚至改成0也是在同一个频率,大概在391MHz左右且无法锁定。目前看似乎更改任何N和R值都无法改变,所以我怀疑是VCO待在了最低频率,是因为环路没有正确设置,如图,我在数据手册中无法找到关于CP MUX,VCO MUX和OP MUX的切换方法,请您告诉我正确的切换方法。(另外,我认为您之前说的寄存器有偏差,例如您说R1和R2是N分频比,但是我使用的是R4寄存器设置整数部分的分频,可能是您看错了器件型号,我正在调试的是LMX2571,谢谢)