Part Number: LMX2595
下变频本振10.6GHz,参考信号50MHz,输出中频2.15GHz时,在2.15GHz附近出现以50NHz为间隔的杂散信号,杂散信号功率固定不变大概在-70dBm,尝试更改参考信号为10MHz时,杂散间隔变为10MHz,经测试为LMX2595输出的杂散,这种杂散属于什么杂散呢?整数边界杂散或者说鉴相杂散?如何降低或者相处此类杂散?谢谢!


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2595
下变频本振10.6GHz,参考信号50MHz,输出中频2.15GHz时,在2.15GHz附近出现以50NHz为间隔的杂散信号,杂散信号功率固定不变大概在-70dBm,尝试更改参考信号为10MHz时,杂散间隔变为10MHz,经测试为LMX2595输出的杂散,这种杂散属于什么杂散呢?整数边界杂散或者说鉴相杂散?如何降低或者相处此类杂散?谢谢!


您好
是否以 TICS Pro 格式共享您的配置? 例如:

是否在 RFout 引脚上使用电阻器或电感器上拉电阻器? 您是否了解10nF 和100pF 电容器的高频特性?
您好
我无法清楚地读取您的配置、您是否已将 RFoutA 功率设置设为1、并将 RFoutB 设为0? 如果您不使用 RFoutB、则应通过 OUTB_PD 位将其禁用。 您是否可以尝试将 RFoutA 功率设置设置为30?