Part Number: CDC3S04
在REQ1和REQ4上拉的情况下,CLK1和CLK4是直接使能输出吗?CLK2和CLK3即便上拉,也是需要通过IIC控制寄存器才可使能的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好

RESET resets REQ1PRIO/REQ4PRIO and REQ1INT/REQ4INT bits to their default values (CLK1/4 is ON) but does not change the remaining internal SW bits. During RESET, any I 2C operation is blocked until RESET is deactivated. A minimum pulse duration of 500 ns must be applied to activate RESET (the internal glitch-filter suppresses spikes of typical 300 ns).
您是对这部有疑问是吗?根据底下辅助说明,关于复位只是复位默认的状态,在复位中,I2C的相关操作会停止,如果您默认是CLk1和CLK4 是输出,那么您复位过程可以让他直接输出,但是在复位期间不允许任何的I2C操作 。