This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDC3S04: 使能上拉问题

Part Number: CDC3S04


在REQ1和REQ4上拉的情况下,CLK1和CLK4是直接使能输出吗?CLK2和CLK3即便上拉,也是需要通过IIC控制寄存器才可使能的吗?

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好

    RESET resets REQ1PRIO/REQ4PRIO and REQ1INT/REQ4INT bits to their default values (CLK1/4 is ON) but does not change the remaining internal SW bits. During RESET, any I 2C operation is blocked until RESET is deactivated. A minimum pulse duration of 500 ns must be applied to activate RESET (the internal glitch-filter suppresses spikes of typical 300 ns).

    您是对这部有疑问是吗?根据底下辅助说明,关于复位只是复位默认的状态,在复位中,I2C的相关操作会停止,如果您默认是CLk1和CLK4 是输出,那么您复位过程可以让他直接输出,但是在复位期间不允许任何的I2C操作 。