想问下DAC900电流输出端可以直接连接电阻吗?对电阻的大小有什么要求。。。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
可以的,DAC900输出为电流源,根据你的应用需要的输出阻抗和电压范围选择电阻。
能否详述你的应用。
Li
可以连接电阻到地,把电流信号转换为电压信号。具体您可以参见手册的第11页。电阻的大小可以参见手册的公式5和6
可以直接连Rload。这个电阻可以直接将输出电流转化为电压信号
如下图所示,用Rset电阻设定基准电流Iref=Vref/Rset.满幅输出电流是基准的32倍,如选2K的Rset,则输出满幅电流为Iout =20mA.
再由公式Vout = Iout • Rload及输出电压的范围要求确定输出电阻。
注意在datasheet的P12页,模拟输出部分,明确说明,为了达到更好的低失真和低噪声效果,优选满幅输出电流为20mA,当然此时的功耗也要高一些。
同样为了达到低失真的目的,要求输出电压幅值不超过0.5V,(输出电流满幅为2mA时,不超过1V),此时对于20mA的最大输出电流,选50电阻。
在高频线路里,50电阻也利于阻抗匹配。