This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC900问题

Other Parts Discussed in Thread: DAC900

想问下DAC900电流输出端可以直接连接电阻吗?对电阻的大小有什么要求。。。。。

  • 你好!

    可以的,DAC900输出为电流源,根据你的应用需要的输出阻抗和电压范围选择电阻。

    能否详述你的应用。

  • Li

    可以连接电阻到地,把电流信号转换为电压信号。具体您可以参见手册的第11页。电阻的大小可以参见手册的公式5和6

  • 可以直接连Rload。这个电阻可以直接将输出电流转化为电压信号

    如下图所示,用Rset电阻设定基准电流Iref=Vref/Rset.满幅输出电流是基准的32倍,如选2K的Rset,则输出满幅电流为Iout =20mA.

    再由公式Vout = Iout • Rload及输出电压的范围要求确定输出电阻。

    注意在datasheet的P12页,模拟输出部分,明确说明,为了达到更好的低失真和低噪声效果,优选满幅输出电流为20mA,当然此时的功耗也要高一些。

    同样为了达到低失真的目的,要求输出电压幅值不超过0.5V,(输出电流满幅为2mA时,不超过1V),此时对于20mA的最大输出电流,选50电阻。

    在高频线路里,50电阻也利于阻抗匹配。

  • 非常感谢!我做三角波发生器。基本已经没什么问题。只是对DAC900的电流输出端接的电阻大小和输出端输出最大电压有所疑问,必进有些地方不是太熟悉,在电路调试过程中出现BUG,我现在用的电阻式50欧姆。暂时未出现其他问题。还有的是25欧姆电阻,这个也不太了解,