Part Number: TPL0102-100
Can I directly connect LA and WB of TPL0102 to achieve 0~200Ω resistance?
Currently, the software is unable to communicate with the module. After writing the device address, there is no ACK response.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPL0102-100
Can I directly connect LA and WB of TPL0102 to achieve 0~200Ω resistance?
Currently, the software is unable to communicate with the module. After writing the device address, there is no ACK response.
Thank you and look forward to your reply.
Thank you and look forward to your reply.
您好,
it was 19K ohms
理论上WA在LA位置(7.6.4 WRA),WB在LB位置(7.6.6 WRB),电阻为0.
实测每个通道的RWL是多少?您回读确认寄存器正确吗?
TPL0102 Two 256-Taps Digital Potentiometers With Non-Volatile Memory datasheet (Rev. C)