Part Number: ADS1299
Hello,there are 2 ways in datasheet about power supply. I want to konw which is the best about EEG acquisition. If AVDD–AVSS max =5.25 means I can use AVDD=2.5V, AVSS= -2.5V or AVDD=1.5V, AVSS= -1.5V ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1299
Hello,there are 2 ways in datasheet about power supply. I want to konw which is the best about EEG acquisition. If AVDD–AVSS max =5.25 means I can use AVDD=2.5V, AVSS= -2.5V or AVDD=1.5V, AVSS= -1.5V ?