This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: The difference between single and dual power supply.

Part Number: ADS1299


Hello,there are 2 ways in datasheet about power supply. I want to konw which is the best about EEG acquisition. If AVDD–AVSS max =5.25 means I can use AVDD=2.5V, AVSS= -2.5V or  AVDD=1.5V, AVSS= -1.5V ?