Part Number: DAC81408
您好,关于DAC81408,在配置其寄存器之前需要做哪些工作?重置阶段需要进行哪些作?复位完成后,写入寄存器时,示波器显示数据正常,但为什么无法读取寄存器中的值?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC81408
您好,关于DAC81408,在配置其寄存器之前需要做哪些工作?重置阶段需要进行哪些作?复位完成后,写入寄存器时,示波器显示数据正常,但为什么无法读取寄存器中的值?
您好
请按照以下说明配置DAC81408输出-
如果SPI通信按预期工作,请尝试以下顺序获取DAC电压输出-
a) 在SPICONFIG中写入0x0A84(0x03)-为DAC81408设备加电
b) 在GENCONFIG(0x04)中写入0x3F00-如果使用内部引用
c) 在DACPWDN中写入0x0000(0x09)-为各个DAC通道加电
d) 在DACn_DATA(n=0x14至0x1B)中写入0x8000,以将单个DAC通道输出配置为2.5 V
重置后,您需要等待至少1ms,然后开始SPI写入。