Other Parts Discussed in Thread: SN75LVDS83B, AM3354
我们用的是18-bit的LCD显示屏,CPU用的是AM3354,因此我们就想利用SN75LVDS83B来实现RGB到LVDS的转换。
同时我看了SN75LVDS83B的datasheet文档,里面也有相应的连接图,但是我有一个地方不是非常明白。在手册的21和22页的连接图都能理解,分别为24-bit对应24-bit, 18-bit对应18-bit. 但是我们的想法是想RGB端接成24-bit,为的就是兼容以后的24-bit的LCD模块。
对于目前我的系统而言就是24-bit 连接18-bit的问题了。那么问题来了,
问题一:我是应该按照第21页的连接图连接呢(不用Y3+/Y3-)还是按照第24页的连接图连呢?
问题二:为什么第24页里面的连接图要奖R0,R1,G0, G1, B0, B1 置成NC呢?而不是将R6,R7,G6,G7,B6,B7置成NC呢?
问题三:因为我们的LCD模块手册里面要求的是R0~R5,G0~G5,B0~B5,如果我按照第24页里面的连接方式连接的话,可不可以将R6,R7,G6,G7,B6,B7换成R0,R1,G0,G1,B0,B1呢?