Part Number: ADS1299
在采样率设置为4K,8K或者16K时,PGA设定为1,输入1kHz正弦波,幅值设定在压摆率容许范围之内,得到结果衰减远超-3dB,大约在-6dB左右。测试信号逐步减小频率发现-3dB在700Hz左右,达不到手册中表注的0.25*fIN/fDR,请问是什么原因
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我采用四片ADS1299,均配置为单端参考模式,即所有的负极连接在一起作为REF,做32通道脑电。
硬件供电正负2.5V,使用外部时钟2.048MHz,外部参考电平相对于负电源为2.5V。BIAS引脚也并联四片,但仅通过第一片的片内运放输出至BISA电极。
软件初始化配置如下:
struct ADS1299_CONFIG ADS1299_Config_Init_Acquire ={
.CONFIG1 = 0xd6, //采样率250Hz
.CONFIG2 = 0xd3, //关闭测试源
.CONFIG3 = 0x7c, //参考和偏置,关闭BIAS脱落
.LOFF = 0x04,
.CHSET[0] = 0x00, .CHSET[1] = 0x00, .CHSET[2] = 0x00, .CHSET[3] = 0x00, .CHSET[4] = 0x00, .CHSET[5] = 0x00, .CHSET[6] = 0x00, .CHSET[7] = 0x00,
.LOFF_SENSP = 0x00,
.LOFF_SENSN = 0x00,
.BIAS_SENSP = 0xff, //从所有通道取共模信号
.BIAS_SENSN = 0x01,
// .MISC1 = 0x20, //连接SRB1和N通道,参考模式 00100000
.MISC1 = 0x00,
.MISC2 = 0x00,
.GPIO = 0x0f,
.CONFIG4 = 0x00
};
测试时采样率分别调整至4k,8k和16k,对第一个通道输入1kHz正弦波,发现有-6dB衰减。