Part Number: ADC3683
各位好:
在ADC3683的手册中提到NSD的典型值是-160dBFS/Hz,测试条件是“fIN = 1.1 MHz, AIN = – 20 dBFS”——我很疑惑,测噪声谱密度的话,为什么不是将输入端的P/N短接起来,而要输入一个功率为-20dBFS的信号?TI为什么会选择这种方式?这种方式与输入端P/N短接起来有何不同?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢回复。
实际上我手头正好有一块ADC3683EVM demo板,并对其性能进行了一些基本的测试,包括SNR和NSD。
在测SNR时,利用RS的FSWP50输出65MHz作为参考时钟(并利用一个65MHz带通滤波器滤波),利用SMA100B输出频率为10MHz、功率为-1dBFS的信号,测得SNR约为80.5dB——较手册典型值差了3dB。
在测NSD时,将输入端P/N短接后,测得NSD在10MHz处约-153.8dBFS/Hz,较手册差了6dB。同时还测了利用SMA100B输出1.1MHz/-20dBFS信号时的在10MHz处的NSD,约-151dBFS/Hz,较手册差了8dB。
——我想问的是,要怎样才能测得尽可能接近手册上描述的指标?对于测试方法以及ADC数据的处理方法,TI是否有相关资料可以提供?