Part Number: ADS131A04
Other Parts Discussed in Thread: ADS1261
你好!
ADS131A04工作在同步从模式时,使用SPI四线接口,DRDY与CS短接,怎么得到AD数据已经转换完成状态?
谢谢!
Daivd
2025-10-4
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
仅当总线上有多个设备时,才应使用同步从属模式。 如果仅使用1x ADS131A04,我建议使用异步中断模式。 这更容易使用,因为这种模式与标准ADC通信最相似。 同步从属模式需要特殊的时钟注意事项才能正常工作
您应将CS设置为LOW并提供正确数量的SCLK,以便在任何模式下从ADS131A04读取数据。 您可以在第9.5.3节(SPI命令定义)中看到,ADC输出转换数据作为每个命令响应的一部分。 例如,如果将单词长度设置为24位,应该提供120个SCLK来读取命令响应的数据=24位+来自所有4个ADC通道的24位数据的24*4=96位。 如果启用CRC或用户定义的单词长度不同,则帧长度会发生变化
我还要指出,更适合此应用的设备是ADS1261,因为此ADC与以前使用的设备非常相似