Part Number: DAC81408
芯片上电后对我输入的信号没有反应,供电引脚供电正常,vio3.3v,vref2.5v,vcc10v,vss-10v, vddvaa为5v,然后按照文档时序设计输入信号输入后没有反应,并且测到TEMPOUT引脚输出为5v,但是按照说明文档里不应该为5v,这是哪里出了问题,下图是我的设计原理图和我的输出时序图.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
是的,VTEMPOUT 是个负温度输出电压,0°时是1.34V,室温的话应小于1.34V.
您的电路图没看出什么问题,请检查PCB设计和焊接。
您的时序图中,CS保持低的时间为24个SCLK下降沿,您展示的是写操作。
建议您试一下读取“9.6.2 DEVICEID Register (Offset = 01h)” 寄存器值来检测芯片已工作和通讯时序。
然后再写入回读的方式确定写时序。
您好,
VTEMPOUT电压正常了吗?
根据数据手册“Table 2. Serial Interface Access Cycle”, 复位命令帧正确。
读01寄存器的命令字:1x00 0001 xxxx xxxx xxxx xxxx,但您的波形来看是: 1001 0100 0000 0000 0000 0000
另外,SCLK是25个脉冲,好似最后一个脉冲时CS已拉高,建议您确认一下SPI MASTER的程序。
对于电路问题如方便,可以测试一下DAC81416-08EVM Evaluation board | TI.com
VTEMPOUT电压貌似正常了,我在重新上电后 VTEMPOUT为5v,之后向SPICONFIG Register (Offset = 03h)寄存器中写入