This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1306E25: sigma-delta ADC和ADR ADC的区别

Part Number: AMC1306E25

hello,

想咨询一下sigma-delta ADC和ADR ADC(逐次逼近型)ADC的区别。

1、AMC1306是78K 采样率,16bit的对吧?那么我用AD7626,采样频率200K,或者更高的,然后经过滤波,得到的数据,会不会比AMC1306更好呢?怎么去评价sigma-delat ADC和逐次逼近型 ADC的性能优劣?(逐次逼近型,我通过提高采样频率,然后进行滤波)

2、伺服驱动器里面,建议用sigma-delta ADC还是高采样率的逐次逼近型ADC?

3、AD1271也是sigma-delta ADC,速率也高些,是否可以替代AMC1306E25呢?

谢谢