ADS1263EVM-PDK: ADS1263 Collection issue

Part Number: ADS1263EVM-PDK
Other Parts Discussed in Thread: ADS1263

I understand what you mean. The input sine wave cannot be bipolar. Should we use a sine wave with a peak-to-peak voltage of 1V and a bias voltage of 2.5V for the input? Is that correct? Our EVM is powered by a single-ended 5V supply. I would like to ask if the ADS1263 chip can be powered by ±2.5V.