Part Number: ADS125H02
我给ADS125H02施加的电源是DVDD=3.3V,AVDD=5V,结果发现DVDD变成了4.1V。这是为什么呢?我断开DVDD供电,单独测量为3.3V,供电正常,但一加到ADS125H02上,就变成了4.1V。我把AVDD不加电的话,DVDD为3.3V,正常。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS125H02
我给ADS125H02施加的电源是DVDD=3.3V,AVDD=5V,结果发现DVDD变成了4.1V。这是为什么呢?我断开DVDD供电,单独测量为3.3V,供电正常,但一加到ADS125H02上,就变成了4.1V。我把AVDD不加电的话,DVDD为3.3V,正常。
DVDD我用DC/DC电源供电,电压值为+3.3V,结果AVDD一加电后,DVDD就变成了4.1V,ADS125H02可能还能忍受,但我的DVDD还接到了其它供电要求3.3V的器件上,如FPGA,而FPGA在4.1V 供电情况下无法正常工作。
您好
不,这并非ADC应有的行为,即正常工作的设备不会加载DVDD引脚。例如,你可以测量ADS125H02EVM的DVDD引脚,其电压应为3.3V而非4V。
这听起来像是系统中某个环节出了问题。可能是焊接问题或供电问题。我建议先将板上的H02设备隔离,然后用台式电源供电。假设模数转换器(ADC)未损坏,你应该能观察到供电稳定。接着,逐步将板级电源重新连接到ADC,观察DVDD何时开始加载