ADS8681: How to achieve 1MSPS with ADS8681?

Part Number: ADS8681

hi,

我需要您的帮助,在使用ADS8681芯片时,无法达到规格书中的1MSPS,最高能到33KSPS,以下是配置信息:

使用ESP32-S3作为控制端,其频率是240MHz,编写一个ADS8681读取数据的最小系统,通过标准 SPI读取ADS8681的数据,SPI的速率是50MHz,ADS8681的量程是:±10.24V,这种情况下,读取的数据是正确的,但是采样率无法到达1M

需要确认的问题是:

1.使用Dual SDO与SRC模式可以提高采样率,于是将SDO_CTL_REG寄存器修改为0x0303,首先,在这种模式下,是否无法读取寄存器的内容来,从而判断是否配置成功,其次,这种模式下,是否判断RVS引脚的电平的方式,来读取SDO-0和SDO-1的数据,最后:这种方式即使将SDO1_CONFIG[1:0]配置为11b,是否只会将33Ksps提升到66Ksps,无法实现到1Msps

这边是否有关于ADS8681芯片1Msps的MCU的例程,请告知我

如果我对ADS8681的使用存在错误,请指正

thanks!!!