This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8665: ADS8665:AVDD关闭(0V)且DVDD为3.3V时AIN_P是否带电

Part Number: ADS8665

TI专家您好,

我在使用ADS8665检测连接至AIN_P引脚的外设模拟信号。系统中:

  • DVDD = 3.3V(常开)

  • AVDD = 5V(可独立关闭)

我观察到,当 AIN_P 引脚处于悬空状态(没有外部外围设备连接时),该引脚上会存在约 1V的电压。根据数据手册以及相关的 E2E 讨论,这是由于器件内部的偏置电压所致。

我的问题是:如果关闭AVDD(置为0V),同时DVDD保持3.3V,能否保证AIN_P引脚上不带电(即0V)?

期待您的解答,谢谢!