This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1258测量方波信号上带有300mv以上直流差分偏置电压时,方波信号有噪声大的问题?

Other Parts Discussed in Thread: ADS1258, OPA2365, OPA2340

我最近使用ADS1258作为心电信号采集芯片,ADS1258使用单电源+5V供电,ADS1258的电路如图

ADS1258使用运放缓冲信号差分输入,通过MUXP,MUXN复用输出到OPA2365组成的差动放大器,放大后进行采样。

ADS1258缓冲运放使用运放OPA2340作为跟随器,通过电阻10K串接输入到ADS1258,如下,

现在测量方波信号,如果直流偏置电压小于150mv时,方波信号很好,基本上没有什么噪声,但是直流偏置信号大于300mV时,采样得到的方波噪声就变大了。

下面图片是我测量150mv,200mv,250mv,300mv,400mv直流偏置+方波信号测量出来的方波信号。

100mv+1mv/2HZ方波

150mv+1mv/2HZ方波

200mv+1mv/2HZ

300mv+1mv/2HZ方波

400mv+1mv/2HZ方波

可以看出明显噪声越来越大。因为这是心电图的一个指标,所以希望能把这个问题解决了。请问以下TI工程师们,各位大神,帮忙分析分析,帮我看看是什么问题的原因呢。有没有什么办法解决?